Analysis Parameters
Analysis Parameters must be set prior to model construction. Once a process model has been constructed, analysis parameters cannot be altered.
Analysis Parameters are accessed from the Options>Analysis Parameters menu.
NOTE: Analysis Parameters can only be changed during Preparation and modeling.
Smoothing window size
This is the moving average filter that is applied to the input tags before they are used in the various model calculations. The default value for this window is 10:00 (10 minutes).
The size of the window is specified using the following format:
dd HH:mm:ss
where
dd = days; HH = hours; mm = minutes; ss = seconds.
Related topics: